Electrical Equipment Rooms
Floors
Sweden

Ryhov County Hospital undergoes renovation

The collaboration between Linjemontage and Bergvik Group is working really well. They are quick to help and find solutions in existing spaces where Iso Floor can be installed in stages so as not to disrupt or compromise personal and operational safety at the hospital. When changes have been made at the construction site, Bergvik has responded at lightning speed to the customer's needs. Heroic efforts and professional project organisation!
Dennis Månsson, Linjemontage

The collaboration between Linjemontage and Bergvik Group is working really well. They are quick to help and find solutions in existing spaces where Iso Floor can be installed in stages so as not to disrupt or compromise personal and operational safety at the hospital. When changes have been made at the construction site, Bergvik has responded at lightning speed to the customer's needs. Heroic efforts and professional project organisation!

Expansion and renewal of power supply

The project is expected to be completed in 2021. Together with our client Linjemontage, Bergvik has been entrusted with supplying Iso Floor installation flooring for these areas. The total area covered by switchgear flooring is estimated at approximately 600 m2. The hospital will be expanded in accordance with a master plan that has been drawn up, in which the first stage of the expansion and modernisation of the hospital is called D1, which includes the addition of more space to meet some of the hospital's increased needs.

CAD - The process

Bergvik's CAD department gets involved at an early stage, designing the floor and suggesting how Bergvik wants the floors to be built to handle the loads involved. This gave Linjemontage the chance to get an early idea of what the solutions would look like and what changes needed to be made to simplify the installation of equipment and ducting. After completion of the installation, documentation is provided so that future users can easily see how the solution is constructed.

Solutions

Bergvik has used different versions of Iso Floor in all areas. The flexibility of Iso Floor allows Bergvik to easily design the floors to suit the equipment available. In this case, integrated transformer stands and transport aisles have been used to roll in and set up the 6,000 kg transformers located in some of the rooms.

Project facts

When Ryhov County Hospital opened in 1988, it was one of Sweden's most modern hospitals. When it became clear that operations were changing faster than the premises could keep up, a master plan was drawn up that included a property development plan. The plan contains strategies and plans for the continued development of the hospital over a 20-30 year period.

This is Ryhov

Ryhov County Hospital in Jönköping has approximately 3,500 employees and is the largest hospital in the county. The hospital was founded in 1988 and was the second most expensive construction project in Sweden during the 1980s. Today, Ryhov consists of 34 departments and has more than 400,000 visits each year.

‍

Related References

Stay updated with articles that explore design, strategy, and innovation. My blog offers tips, case studies, and reflections on the latest trends and best practices in the industry.

Electrical Equipment Rooms
Floors
Bravida, Förbifart Stockholm - A great connection
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
Henrik Sundström, Production Manager for Förbifart Stockholm at Bravida
Data Centre
Floors
Availo Data Center, Stockholm
Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.
Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.
Erik Kjellin, Projekt Manager, Availo Networks