Data Centre
Floors
Sweden

Availo Data Center, Stockholm

Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.
Erik Kjellin, Projekt Manager, Availo Networks

Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.

Erik Kjellin lists the main advantages of Iso Floor:

  • Flexible design.
  • The size of the floor tiles was adapted to our server racks, which meant that we did not lock any floor tiles in front of or behind the server racks.
  • All floor tiles can be removed without compromising the stability of the floor.
  • Ample space under the floor for cable routing, not a ‘forest’ of leg supports like conventional installation floors. Cable ladders are mounted on brackets, which are easily attached to the floor legs.
  • No expensive welded steel frames were needed for HVAC, UPSs and electrical equipment; these were simply placed on the Iso Floor construction.
  • We also used Iso Floor for all electrical rooms in the same project.The order included construction drawings so that we could easily plan other installations.
  • Easy to adjust and reinforce, should point reinforcement be required in the future.
  • Half the installation time compared to traditional installation floors.

Project facts

Availo Datacenter is built with the latest technology to minimise power losses and with the environment in mind. Availo's facilities maintain a very high standard when it comes to power supply, cooling, security and fire protection. The data centre has the ability to deploy backup power in the form of diesel generators for each electrical system, to ensure continued operation in the event of a power failure.

This is Availo

Availo was founded in 2011 but has experience dating back to the early days of the internet in the 1990s. Since 2014, the Availo Group has been owned by IP-Only AB, which operates in the field of internet/telecom infrastructure and services for businesses, private individuals and municipalities.

Related References

Stay updated with articles that explore design, strategy, and innovation. My blog offers tips, case studies, and reflections on the latest trends and best practices in the industry.

Electrical Equipment Rooms
Floors
Bravida, Förbifart Stockholm - A great connection
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
Henrik Sundström, Production Manager for Förbifart Stockholm at Bravida
Data Centre
Floors
Eco Datacenter, Falun
Bergvik Group AB has been honoured to supply installation flooring to EcoDataCenter in Falun. This is the world's greenest data centre!
Bergvik Group AB has been honoured to supply installation flooring to EcoDataCenter in Falun. This is the world's greenest data centre!