Electrical Equipment Rooms
Floors
Sweden

Flooring in two stages for Brittedal, Hästveda

The contact with Bergvik has been excellent and they were very accommodating from the initial contact until everything was finalised. The project has been a complex puzzle involving many parties, but Bergvik has adhered to the schedule and promised deliveries very well and entirely according to plan.
Anders Viberg, CEO, Brittedal

The contact with Bergvik has been excellent and they were very accommodating from the initial contact until everything was finalised. The project has been a complex puzzle involving many parties, but Bergvik has adhered to the schedule and promised deliveries very well and entirely according to plan.

Bergvik delivers and installs flooring in two stages for Brittedal

After the electricity network company Brittedal in Hästveda took over an old station in poor condition, Bergvik Group AB was given the opportunity to supply new flooring for the project.

Brittedal is starting by refurbishing the old building and has decided to build a new switchgear in the old building. The old switchgear in the building was constructed with a rail bridge between two switchgear sides. This made it possible, after an operational interruption, to move the load to one side and open the rail bridge to de-energise and demolish one side. When the new installation floor is to be installed, it must be done in two stages.

Stage one

Bergvik Group is supplying and installing flooring for Brittedal in two stages, with the first stage involving the construction of half the surface area so that a new 10 kV switchgear can be built and the cables installed. Once the substation was complete, operations were transferred to the new facility and the remaining half of the old substation could be demolished.

Stage two

In stage two, a new 24 kV switchgear was built to replace the old one, which was located outdoors. The second stage was a little more complicated due to the size of the switchgear and the doorways in the old building. Once the switchgear was in place, Bergvik Group had to return a third time to install the frame and railings

Project facts

At the turn of 2018/2019, Brittedal took over a station from E.ON that was in very poor condition. There were two options: either demolish it or build a new one. The building was made of brick and in a condition that could be refurbished, so this option was chosen over demolition and rebuilding. The building was refurbished both inside and out, and a new substation was built in the old building.

This is Brittedal

Brittedal is an electricity network company covering a large geographical area that extends across the municipalities of Hässleholm, Osby, Östra Göinge and Kristianstad. Brittedal is an economic association and is therefore owned by its members.

‍

Related References

Stay updated with articles that explore design, strategy, and innovation. My blog offers tips, case studies, and reflections on the latest trends and best practices in the industry.

Electrical Equipment Rooms
Floors
Bravida, Förbifart Stockholm - A great connection
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
Henrik Sundström, Production Manager for Förbifart Stockholm at Bravida
Data Centre
Floors
Availo Data Center, Stockholm
Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.
Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.
Erik Kjellin, Projekt Manager, Availo Networks