Data Centre
Floors
Sweden

Eco Datacenter, Falun

Bergvik Group AB has been honoured to supply installation flooring to EcoDataCenter in Falun. This is the world's greenest data centre!

Bergvik Group AB has been honoured to supply installation flooring to EcoDataCenter in Falun. This is the world's greenest data centre!

An obvious choice

Bergvik Iso Floor was the obvious choice of installation flooring for ECO DC. Bergvik Iso Floor's strength lies in its ability to be adapted for heavy loads, customised equipment and demanding spaces. In data centre environments, it is not uncommon to require large quantities of cooling pipes and other bulky equipment that can be difficult to fit under the raised floor. At Bergvik, we are experts in this field. Together with the customer, our skilled designers designed the project in a CAD environment, which makes it easy to coordinate with projects under construction in order to identify and rectify any problems. Bergvik Sweden AB manufactures the entire floor itself, from floor tiles to leg supports, which allows the design of the floor to be adapted so that it can always be optimally adapted to the space and equipment.

Project facts

Construction of the project began in 2018 in Falun and was completed later that year. The data centre is climate positive and runs solely on renewable energy. It has a very high energy efficiency rating, with a PUE of 1.15! Bergvik was involved in this innovative and environmentally friendly project from the outset, supplying and installing our raised access flooring for data centres.

This is EcoDataCenter

EcoDataCenter builds and operates world-class climate-positive data centres for colocation and HPC. It is the world's greenest data centre solution. The first facility is located in Falun and is integrated into the energy ecosystem with Falu Energi och Vatten.

Related References

Stay updated with articles that explore design, strategy, and innovation. My blog offers tips, case studies, and reflections on the latest trends and best practices in the industry.

Electrical Equipment Rooms
Floors
Bravida, Förbifart Stockholm - A great connection
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
"In a project this complex, with so many people involved and sometimes extremely tight schedules, it is a major advantage to work with people who genuinely want to find solutions and do everything they can to deliver. Bergvik is accommodating, incredibly flexible, and everyone is focused on solving the problems that arise."
Henrik Sundström, Production Manager for Förbifart Stockholm at Bravida
Data Centre
Floors
Availo Data Center, Stockholm
Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.
Since 2006, Bergvik Group has been our go-to supplier for raised access flooring in our data centres. They deliver very high quality in terms of both materials and service, and I am convinced that their Iso Floor construction will become standard in all data centres, just as it already is in electrical rooms.
Erik Kjellin, Projekt Manager, Availo Networks