Data Centre
Floors
North America
Other Europe
Sub-Saharan Africa
Asia-Pacific

Data Realty, South Bend, USA

The biggest advantage that we are realizing is the flexibility using Bergvik’s custom size floor panels. We added more Rack rows per square foot (increasing our density) by going with 915 mm cold aisles. We also went with 1220 mm hot aisles, but have dropped those where applicable on an ’as needed’ basis.
Tom Panozzo, CTO, Data Realty

The biggest advantage that we are realizing is the flexibility using Bergvik’s custom size floor panels. We added more Rack rows per square foot (increasing our density) by going with 915 mm cold aisles. We also went with 1220 mm hot aisles, but have dropped those where applicable on an ’as needed’ basis.

"Only bergvik could provide the kind of server rackdensity we needed"

That is how Tom Panozzo, CTO at Data Realty in South Bend IN, describes how Bergvik’s Iso Floor helped make their data center flexible.

Bergvik solved Data Realty’s special need for optimization by manufacturing additional custom floor panels in sizes; 50” x 24”, 44” x 24”, 28” x 24” – and delivered them within 5 weeks.

”I know of no other flooring system that would allow me to reconfigure my floor to suit individual (future and unforeseen) client requests without also rebuilding the floor substructure at extreme cost. With Bergvik, I just order custom sized panels and I am done... No substructure work, no contractors, no cost beyond panels. When I consider that with competitor flooring systems reconfiguration is extremely costly and in most cases impossible, I consider this to be the biggest benefit,”
says Tom Panozzo, CTO at Data Realty.

Project facts

The mission from Data Realty to Bergvik was to provide them with a flexible raised floor solution that would allow them to change the Server Rack pitch at any stage, depending on Rack size and which type of customer would move in. General Contractor was Turner Construction. Raised Floor area was 7340 ft2 (682 m2) and UDL Loading 300 PSF (13.5 kN/m2. The time for installation was only 5 days. Ron Sinopoli, Turner Construction said; "I have never seen a raised floor installed so quickly!".

This is Data Realty

Data Realty’s world-class data centers are designed to enable analytic computation on data sets housed within their secure environment. Go to www.data-realty.com for more information.

‍

‍

Related References

Stay updated with articles that explore design, strategy, and innovation. My blog offers tips, case studies, and reflections on the latest trends and best practices in the industry.

Electrical Equipment Rooms
Floors
911 Dispatch Center, Harford County, USA
The mission from Harford County Emergency Services to Bergvik was to install an aesthetically pleasing, quality raised floor with a fully lateral stable sub-structure and only 1/3 as many pe­destals to avoid obstructions and speed up installation.
The mission from Harford County Emergency Services to Bergvik was to install an aesthetically pleasing, quality raised floor with a fully lateral stable sub-structure and only 1/3 as many pe­destals to avoid obstructions and speed up installation.
Data Centre
Floors
Bergvik provides Iso Floor for Vodacom, South Africa
We do not hesitate recommending the Bergvik Iso Floor system and thank Bergvik for the excellent support rendered to Vodacom on our development projects.
We do not hesitate recommending the Bergvik Iso Floor system and thank Bergvik for the excellent support rendered to Vodacom on our development projects.
Vodacom