Sandvik Coromant, Gimo - A successful partnership with Bergvik

The floor plates can be quickly and easily lifted to provide access to cables and other items under the floor, allowing technical staff to quickly fix problems without disrupting production. This flexibility helps keep operations running with minimal disruption.
Mattias Nyström
Electrical Safety Manager at Sandvik Coromant
Focus on efficiency and consistency - Sandvik Coromant's long-term partnership with Bergvik
Since 2000, Sandvik Coromant has chosen to use Bergvik products for its facilities, and today more than 1,200 square meters of grid access floors are installed. This long-standing relationship has proven to be very successful, especially when it comes to refurbishing existing systems and carrying out new construction.
One of the biggest advantages of Bergvik products is the simplicity and agility they offer in daily work.
- The floor plates can be quickly and easily lifted to provide access to cables and other items under the floor, allowing technical staff to quickly fix problems without disrupting production. This flexibility helps keep operations running with minimal disruption,” says Mattias Nyström, Electrical Safety Manager at Sandvik Coromant.
For Sandvik Coromant, it has also been important to create uniformity in its facilities. By using the same type of grid access floor from Bergvik everywhere, it becomes much easier to maintain, upgrade and replace parts when needed. This saves both time and resources, while simplifying the management of spare parts. Since all facilities are equipped with the same floor type, the need to keep a large and varied stock of spare parts is reduced, allowing maintenance planning and inventory management to be optimized.
PROJECT FACTS
Sandvik Coromant has a continuous need for Bergvik's products, and the cooperation has been ongoing since 2000 and continues to be long-term. When a new build or upgrade of a grid access floor is required, Sandvik contacts its distributor, who in cooperation with Bergvik develops the best solution for the space and the specific needs.
This is Sandvik Coromant, Gimo, Sweden:
Sandvik Coromant in Gimo is one of Uppsala County's largest private employers with approximately 1200 employees. Together with customers and partners, Sandvik Coromant is leading the way towards a sustainable future, delivering tooling solutions to the world's manufacturing industries. Over eight decades of practical experience has provided a wealth of knowledge in metalworking and machining. Sandvik Coromant owns over 1700 patents worldwide, launches over 2500 new products per year, employs approximately 8 000 people and is represented in 150 countries. Sandvik Coromant is part of the Sandvik Group.